AnsweredAssumed Answered

How to update settings with CubeMX in a project that is already opened?

Question asked by TSK on Jun 4, 2015
Latest reply on Jun 4, 2015 by TSK
I generated init code using STM32CubeMX and it turned out I wanted to map some IOs differently. I modified the settings and clicked the generate source code button and it of course it didn't just update my project files but rather generated a new project so I had to do a lot of re-work. Is there (I hope there is!) a way to modify settings and just update the project files without doing additional modifications so I won't have to do a lot of fixing up each time?

Outcomes