AnsweredAssumed Answered

STM32Cube_FW_F3_V1.1.0 stm32f3xx_hal_uart.h: line 444: missing closing bracket

Question asked by pretzsch.andreas on May 28, 2015
Latest reply on Jun 1, 2015 by Amel N
In STM32Cube_FW_F3_V1.1.0 (same with V1.1.1) in file
  Drivers/STM32F3xx_HAL_Driver/Inc/stm32f3xx_hal_uart.h
there is a closing bracket missing on line 444:
 435 /** @defgroup UART_Flags     UART Status Flags
 436   *        Elements values convention: 0xXXXX
 437   *           - 0xXXXX  : Flag mask in the ISR register
 438   * @{
 439   */
 440 #define UART_FLAG_REACK                     ((uint32_t)0x00400000)
 441 #define UART_FLAG_TEACK                     ((uint32_t)0x00200000)
 442 #define UART_FLAG_WUF                       ((uint32_t)0x00100000)
 443 #define UART_FLAG_RWU                       ((uint32_t)0x00080000)
 444 #define UART_FLAG_SBKF                      ((uint32_t)0x00040000 
 445 #define UART_FLAG_CMF                       ((uint32_t)0x00020000)
 446 #define UART_FLAG_BUSY                      ((uint32_t)0x00010000)
 [...]

Outcomes