AnsweredAssumed Answered

STM32F3xx and Ulink2 Debugger

Question asked by elpel.marc on May 20, 2015
Latest reply on May 21, 2015 by Clive One
Using a ULink2 debugger I can download code OK, but debugging is marginal to non-functional.  I found if I press the hardware reset AFTER entering the "Start Debug Session", I can usually get 1-break point to work reasonably well.  I've heard the ULink2 should use an *.ini file for proper configuration to the application, but can find no details or examples or any information which would be in that ini file.  Suggestions...?

Outcomes