AnsweredAssumed Answered

Iusse of System bootloader of STM32F0 with Flash Loader Demonstator

Question asked by thieu.toan on Sep 27, 2012
Latest reply on Mar 14, 2013 by beniamino.giorgio
Dear Friends.

Does anyone use Flash loader Demonstrator for STM32F0? I try out and work hard 2 days for boot loader of STM32F0 with Flash demonstrator but It is still not working. I'm using STM32F0DISCOVERY. I set boot 0 is high leve with 10K pull up. I try how to use boot loader with evaluation board STM32F1, STM32F2 are always successful.

I don't know we need to set BOOT1. I see in AN2606 setting BOOT 1 pin is optional bytes. Anyone help me how can to do that.




 

Outcomes