AnsweredAssumed Answered

tim4 not work with STM8S103K3

Question asked by Pol on Jan 7, 2016
Latest reply on Jan 8, 2016 by Pol
Hello:

I'm write code from STM8S105C4T6 using tim4 basic timer, the code is store  in INTERRUPT_HANDLER routine, anythings work.

I'm change to use  STM8S103K3T6C (smallest) , the interrupt routine don't fire,
I change from tim4 to tim1, everythings work.

I'm alway read the datasheet of STM8S103, it's also had tim1, tim2 and tim4

Why can't use it, anyone can explain this ?

Outcomes