AnsweredAssumed Answered

ST-LINK files for M29W128 External Loader for F407

Question asked by Moore.Patrick on Apr 14, 2015
Latest reply on Apr 22, 2015 by Clive One
I have an application with a F407 that has a correctly working M29W128 that happens to be on NE1 (so the starting address is 0x60000000).  The application works wonderfully using a resident bootloader that accepts a large file via Ethernet that fills the balance of the internal F407 flash and then "overflows" into the external M28W128 as needed.

For production, it would be easier if I could load the external flash via SWD using the ST-LINK, but the ST-LINK software does not seem to have pre-existing loader for my configuration.  The ST-LINK Utility 3.6.0 documentation tells me how to create my own loader, but the directory with the source code for the M29W128 is empty.  The other three other memory types are fully populated with files. 

Does anyone know where I might be able to find the ST-LINK external loader code examples for the M29W128?

Outcomes