AnsweredAssumed Answered

Trouble using Tasking toolset

Question asked by vivek on Sep 17, 2012
Latest reply on Sep 17, 2012 by Clive One
Hello every1,
            I've been using the keil MDK compiler for a long time. Due to some circumstances i have to use Altium Tasking toolset. As i was trying to compile one of the peripheral example(Flash Program) i got the following errors

1. lkarm E108: multiple definitions of symbol "_START" in both "cstart.obj" and "cstart_thumb2.obj"
2. amk E452: target 'FLASH_Program.abs' returned exit code 1

These errors remains the same for any example program. But i did not get these error when i used Keil MDK. Any hep wud be appreciated.

FYI: Im using STM32F4 discovery board.

Outcomes