AnsweredAssumed Answered

STemWin and external RAM

Question asked by szymura.michal.001 on Apr 2, 2015
Latest reply on Aug 21, 2017 by barge.somnath
I have linked STemWin library. My project uses external RAM.
When I display some progressbar using internal RAM, value of progress is displayed correctlly (ex. 50%). When I am switching buffer "aMemory" to extrernal RAM (static U32 aMemory[GUI_NUMBYTES / 4] __attribute__ ((section(".extram"))) the value of progress is displayed strange, ex. 00 instead off 50%, 33 instead of 13%, each times the second digit is shown twice, first digit and "%" char aren't displayed.
Where is the problem ?

Outcomes