AnsweredAssumed Answered

SPI3 not working

Question asked by Kilohercas on Sep 5, 2012
Latest reply on Mar 13, 2013 by jin.xin
Hello, ai am trying to comunicate with external DAC and having some hard time using SPI3 in GPIOC port (12,10 and 11 for CS)
i have no problem with SPI2, but SPI2 is for LCD touschreen so i want to make new one;

so far i found mistake in standartlib:
*          ===================================================================
*                                 How to use this driver
*          ===================================================================
*   
*          1. Enable peripheral clock using the following functions
*             RCC_APB2PeriphClockCmd(RCC_APB2Periph_SPI1, ENABLE) for SPI1
*             RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI2, ENABLE) for SPI2
*             RCC_APB1PeriphResetCmd(RCC_APB1Periph_SPI3, ENABLE) for SPI3.

so far code looks like this, CS is working but no CLK or MOSI (i need just Tx)
  GPIO_InitTypeDef   GPIO_InitStructure;
 
RCC_APB1PeriphClockCmd(RCC_APB1Periph_SPI3,   ENABLE);
RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOC , ENABLE);
 
/*!< SPI pins configuration *************************************************/
 
/*!< Connect SPI pins to AF5 */ 
GPIO_PinAFConfig(GPIOC,  GPIO_Pin_12,  GPIO_AF_SPI3 );
GPIO_PinAFConfig(GPIOC,  GPIO_Pin_10,  GPIO_AF_SPI3);
 
GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF;
GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz;
GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
GPIO_InitStructure.GPIO_PuPd  = GPIO_PuPd_DOWN;
       
/*!< SPI SCK pin configuration */
GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12;
GPIO_Init(GPIOC, &GPIO_InitStructure);
 
/*!< SPI MOSI pin configuration */
GPIO_InitStructure.GPIO_Pin =  GPIO_Pin_10;
GPIO_Init(GPIOC, &GPIO_InitStructure);
 
 
  GPIO_InitStructure.GPIO_Pin =  GPIO_Pin_11;
  GPIO_InitStructure.GPIO_Mode = GPIO_Mode_OUT;
  GPIO_InitStructure.GPIO_OType = GPIO_OType_PP;
  GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_UP ;
  GPIO_Init(GPIOC, &GPIO_InitStructure);
   
 
SPI_InitTypeDef  SPI_InitStructure;
GPIO_SetBits(GPIOC, GPIO_Pin_11);
/*!< SPI configuration */
 
SPI_InitStructure.SPI_Direction = SPI_Direction_1Line_Tx;
SPI_InitStructure.SPI_Mode = SPI_Mode_Master;
SPI_InitStructure.SPI_DataSize = SPI_DataSize_16b;
SPI_InitStructure.SPI_CPOL = SPI_CPOL_High;
SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge;
SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;
SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_128;
SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_MSB;
SPI_InitStructure.SPI_CRCPolynomial = 7;
SPI_Init(SPI3, &SPI_InitStructure);
 
SPI_Cmd(SPI3, ENABLE);

for transmit 16b integer i use:
GPIO_ResetBits(GPIOC, GPIO_Pin_11);
while (SPI_I2S_GetFlagStatus(SPI3, SPI_FLAG_TXE) == RESET)
{}
SPI_I2S_SendData(SPI3, output);
GPIO_SetBits(GPIOC, GPIO_Pin_11);
any ideas why i have no CLK or MOSI output
i am using STM32F417VGT6 144 pin

Outcomes