AnsweredAssumed Answered

IEC60335 problem with COSMIC linker

Question asked by tasca.davide on Jan 26, 2015
Hi everybody,

I'm trying to include in my project the IEC60335 library to have class B self test.

I receive this error during linker phase

#error clnk Debug\stm8s105.lkf:1 segment .CLASS_B_REV size overflow (4)
 The command: "clnk -lC:\Programmi\COSMIC\CXSTM8_32K\Lib  -o Debug\stm8s105.sm8 -mDebug\stm8s105.map Debug\stm8s105.lkf " has failed, the returned value is: 1
exit code=1.

I'm using STM8S105C6 micro and COSMIC compiler (32K free version).

I have tried to replicate what is reported in the .lkf in the example provided with the IEC60335 library, but it doesn't work.


Has anyone found this problem?

Thanks

Outcomes