AnsweredAssumed Answered

STM32F4 Discovery USB Host example (Beagle USB 480)

Question asked by Tim Michals on Mar 27, 2015
Compiled and downloaded the FatFS_USBDisk to the board and it verified the file is written to the USB flash disk and the LED is green.  Also, reconnected several times and validate the LED 3 goes green each time.
 
Attempting to trace the USB traffic using a Beagle USB 480, no traffic is captured, it just shows <Host disconnected>  But, the example works with out an issue. Is there a clocking issue?
(The example works when the USB flash stick is connected to the Beagle USB 480 also)

Verified the USB Beagle is working and able to capture traffic.

Outcomes