AnsweredAssumed Answered

STM32CubeMX configuration bug report

Question asked by just4you on Mar 18, 2015
Latest reply on Mar 30, 2015 by Amel N
I use the STM32CubeMX.

However, it has a wrong configuration problem for UART.

I want to use the asynchronous RX only mode, but it's not configurable.

My configuration procesures:
1. Configuration -> Peripherals -> UART4 as Asynchronous
    Then 2 pin is set as UART4_TX, UART4_RX
2. I want to use the RX only, so I disable the TX pin.
   Then the UART4 configuration is changed as Disable.

As a result, I can't configure as Asynchronous RX only mode.

Outcomes