AnsweredAssumed Answered

The exact mean of "USE_RTOS"

Question asked by guo.xinwen on Mar 13, 2015
In the CubeMX generated code, I found this macro "USE_RTOS", in the implementation of HAL_LOCK macro. And the comment " USE_RTOS should be 0 in the current HAL release ". But now I'm using FreeRTOS. So I need to check if there will be some problem if using FreeRTOS with the HAL layer.
The Chip of my project is STM32F103RC.

Outcomes