AnsweredAssumed Answered

STVP use for more than serial number string

Question asked by stevens.mike on May 28, 2014
Latest reply on Jun 2, 2014 by laurent_l
We use STVP (v3.3.1) for programming parts.  I'm in the process of adding the Serial Number, using that feature in STVP. 
But we have a number of stations, and so each has unique identifying information.  For example, I want to put the following string in EEPROM if from station 1 at site 2: "0102xxxx" where xxxx is the serial number generated by STVP.
For station 2, at site 2: "0202xxxx" where XXXX is a similarly generated independent serial number - the station number and/or location number makes it unique.

So the problem is: is there a command line interface or script method of getting station and location specific information into STVP for programming to an EEROM location???
If so, how do I do this?

Outcomes