AnsweredAssumed Answered

STMCubeMX STM32F411RE MX_DMA_Init()

Question asked by riggs.rob on Mar 10, 2015
Latest reply on Mar 18, 2015 by STM32Cube-T
I have created an STMCubeMX project for the STM32F411RE Nucleo board and it is going pretty well until I tried to use DMA.  I do not get very far because in no case does the MX_DMA_Init() function get created.  The function is declared at the top and called in main(), but it is never defined.  This happens whether I set up DMA for ADC1 or for UART2 TX or for both of them at the same time.

This seems like a fairly fundamental problem to be having.  Has anyone else encountered this or know of a solution?  I am running the standalone STM32CubeMX 4.6.0 with STM32F4 package version 1.4.0.  I am running this on Linux and generating source for TrueStudio 4.3.1.  (I am building on Eclipse with the GNU ARM Eclipse plugin.)


Outcomes