AnsweredAssumed Answered

Using the PXS_RFIN as GPIO

Question asked by john.001 on Dec 5, 2013
Latest reply on Dec 5, 2013 by john.001
Hello
I am using the STM8TL touch IC and need to use the PXS_RFIN pin as an IO to drive a LED ie PA7. If I disable the Prox engine then the LED can be toggled, but if I enable the Prox engine then the LED can not be toggled anymore...
The PXS_CR2, NOISEDETEN bit is disabled. Are the any other bits I must set to use the PXS_RFIN pin as a GPIO?

Thanks
John

Outcomes