AnsweredAssumed Answered

make: *** [build/obj/boot.o] Error 2

Question asked by Aurelien.Leclercq on Jul 7, 2014
Latest reply on Jul 10, 2014 by Aurelien.Leclercq
Hi,
I hope this error is common for Eclipse users...
Directly after installing SPC5 Studio V3 and setting up the one-year licence, I'm able to get all SPC56EL60L5 examples from the SPC5 Studio Wizard working (on the board, CAN not in loop mode, ADC...). But it seems that I click somewhere I should not because it always ends after some time (PC reboot, app restart...) with the below compiler errors. My target is SPC56EL60L5. I also noticed that the Wizard is not available anymore (File->New and toolbars).

It sometimes compiles again after reboot, or combinaison of clear project/generate/build... I can't get it...

The make command in a DOS window returned the error "libintl3.dll is missing" so I installed it. Now the command "make --version" gives:

GNU Make 3.81
Copyright (C) 2006 Free Software Foundation, Inc.
This is free software; see the source for copying conditions.
There is NO warranty; not even for MERCHANTABILITY or FITNESS FOR A
PARTICULAR PURPOSE.

This program built for i386-pc-mingw32


Is it correct? mingw32??? is it coming from the dll I found?


This is the SPC5 Studio output console (same for my projet and all Wizard examples...). The object files are effectively not generated (build/obj folder empty). Any help is welcome.

14:12:13 **** Build of configuration Default for project TRUNK ****
make -j4 all
Compiling boot.s
Compiling crt0.s
process_begin: CreateProcess(NULL, ppc-vle-gcc -x assembler-with-cpp -c -mcpu=e200zx -meabi -msdata=none -mnew-mnemonics -mregnames -mvle -Wa,-amhls=build/lst/boot.lst -DPPC_USE_VLE=1 -MD -MP -MF .dep/boot.o.d -I. -IC:/SPC5Studio/eclipse/plugins/org.chibios.spc5.components.spc5hal_1.0.0.201405131114/component/lib/include -IC:/SPC5Studio/eclipse/plugins/org.chibios.spc5.components.hal.platform.spc56elxx_1.0.0.201405131114/component/lib/include -IC:/SPC5Studio/eclipse/plugins/org.chibios.spc5.components.osal.spc56elxx_1.0.0.201405131114/component/lib/include -I./components/spc56elxx_platform_component/cfg -I./components/portable_spc5_hal_component/cfg -I./components/spc56elxx_hal_board_initialization_component/cfg -I./components/spc56elxx_hal_drivers_component/cfg -I./components/spc56elxx_osal_component/cfg -I./components C:/SPC5Studio/eclipse/plugins/com.st.tools.spc5.components.platform.spc56elxx_1.0.0.201405131114/component/lib/src/boot.s -o build/obj/boot.o, ...) failed.
make (e=2): Le fichier spécifié est introuvable.

make: *** [build/obj/boot.o] Error 2
make: *** Waiting for unfinished jobs....
process_begin: CreateProcess(NULL, ppc-vle-gcc -x assembler-with-cpp -c -mcpu=e200zx -meabi -msdata=none -mnew-mnemonics -mregnames -mvle -Wa,-amhls=build/lst/crt0.lst -DPPC_USE_VLE=1 -MD -MP -MF .dep/crt0.o.d -I. -IC:/SPC5Studio/eclipse/plugins/org.chibios.spc5.components.spc5hal_1.0.0.201405131114/component/lib/include -IC:/SPC5Studio/eclipse/plugins/org.chibios.spc5.components.hal.platform.spc56elxx_1.0.0.201405131114/component/lib/include -IC:/SPC5Studio/eclipse/plugins/org.chibios.spc5.components.osal.spc56elxx_1.0.0.201405131114/component/lib/include -I./components/spc56elxx_platform_component/cfg -I./components/portable_spc5_hal_component/cfg -I./components/spc56elxx_hal_board_initialization_component/cfg -I./components/spc56elxx_hal_drivers_component/cfg -I./components/spc56elxx_osal_component/cfg -I./components C:/SPC5Studio/eclipse/plugins/com.st.tools.spc5.components.platform.spc56elxx_1.0.0.201405131114/component/lib/src/crt0.s -o build/obj/crt0.o, ...) failed.
Compiling ivor.s
Compiling vectors.s
make (e=2): Le fichier spécifié est introuvable.

make: *** [build/obj/crt0.o] Error 2
process_begin: CreateProcess(NULL, ppc-vle-gcc -x assembler-with-cpp -c -mcpu=e200zx -meabi -msdata=none -mnew-mnemonics -mregnames -mvle -Wa,-amhls=build/lst/ivor.lst -DPPC_USE_VLE=1 -MD -MP -MF .dep/ivor.o.d -I. -IC:/SPC5Studio/eclipse/plugins/org.chibios.spc5.components.spc5hal_1.0.0.201405131114/component/lib/include -IC:/SPC5Studio/eclipse/plugins/org.chibios.spc5.components.hal.platform.spc56elxx_1.0.0.201405131114/component/lib/include -IC:/SPC5Studio/eclipse/plugins/org.chibios.spc5.components.osal.spc56elxx_1.0.0.201405131114/component/lib/include -I./components/spc56elxx_platform_component/cfg -I./components/portable_spc5_hal_component/cfg -I./components/spc56elxx_hal_board_initialization_component/cfg -I./components/spc56elxx_hal_drivers_component/cfg -I./components/spc56elxx_osal_component/cfg -I./components C:/SPC5Studio/eclipse/plugins/org.chibios.spc5.components.osal.spc56elxx_1.0.0.201405131114/component/lib/src/ivor.s -o build/obj/ivor.o, ...) failed.
make (e=2): Le fichier spécifié est introuvable.

make: *** [build/obj/ivor.o] Error 2
process_begin: CreateProcess(NULL, ppc-vle-gcc -x assembler-with-cpp -c -mcpu=e200zx -meabi -msdata=none -mnew-mnemonics -mregnames -mvle -Wa,-amhls=build/lst/vectors.lst -DPPC_USE_VLE=1 -MD -MP -MF .dep/vectors.o.d -I. -IC:/SPC5Studio/eclipse/plugins/org.chibios.spc5.components.spc5hal_1.0.0.201405131114/component/lib/include -IC:/SPC5Studio/eclipse/plugins/org.chibios.spc5.components.hal.platform.spc56elxx_1.0.0.201405131114/component/lib/include -IC:/SPC5Studio/eclipse/plugins/org.chibios.spc5.components.osal.spc56elxx_1.0.0.201405131114/component/lib/include -I./components/spc56elxx_platform_component/cfg -I./components/portable_spc5_hal_component/cfg -I./components/spc56elxx_hal_board_initialization_component/cfg -I./components/spc56elxx_hal_drivers_component/cfg -I./components/spc56elxx_osal_component/cfg -I./components C:/SPC5Studio/eclipse/plugins/org.chibios.spc5.components.osal.spc56elxx_1.0.0.201405131114/component/lib/src/vectors.s -o build/obj/vectors.o, ...) failed.
make (e=2): Le fichier spécifié est introuvable.

make: *** [build/obj/vectors.o] Error 2

14:12:17 Build Finished (took 3s.541ms)

 

Outcomes