AnsweredAssumed Answered

TSV632 - negative input current allowed?

Question asked by fried.christian on Jun 27, 2013
Latest reply on Jul 4, 2013 by fried.christian
Hello,

the datasheet for the OpAmp TSV632 allows a maximum input current of 10mA (page 4).
There's no sign given, so I suppose negative input currents aren't allowed.. But I'm not sure and it would help me, if they would be allowed..
So, could someone clarify this, please?

I have series resistors in front of the inputs which would limit the input current to -0.6mA in the worst case.. But I also noticed the input voltage dropping under the allowed Vcc- -0,2V, so it looks for me as current limiting is not enough and I also have to limit the voltage..


Thanks in advance,
Christian

Outcomes