AnsweredAssumed Answered

SPC5-UDESTK Serial Console ?

Question asked by adams.stuart on Sep 23, 2014
Latest reply on Sep 24, 2014 by Erwan Y
I am using UDE 4.2.05 with the SPC560B-DIS (which has UDE debug hardware built in)
I can load and run code via JTAG but ...

How do I access the serial port connection to the target device ???

The target microcontroller UART is connected to the FTDI USB/serial/JTAG device but
I do not see a COM port show up on the PC for the target USB/serial connection.

Should this show up as a COM port or perhaps in a UDE window ??

Outcomes