AnsweredAssumed Answered

STM32CubeMX Clock Configuration Problem

Question asked by stringer.jeff on Mar 4, 2015
Latest reply on Mar 5, 2015 by Clive One
I'm trying to use Cube for an STM32F042 project and I'd like the APB1 peripheral clock to be 1 MHz but Cube is saying that the minimum APB1 peripheral clock is 10 MHz.  Is this true or is this a problem with Cube?  If it does need to be 10MHz or higher where does it say this in the documentation, I couldn't find it.

I've included a screen shot of the parameters and the red box.

Thanks,
Jeff



Attachments

Outcomes