AnsweredAssumed Answered

STM32CubeMX: CRC peripheral missing for STM32F2xx MCUs

Question asked by Thosch on Mar 4, 2015
Latest reply on May 8, 2015 by Thosch
Hi all,

I'm using the STM32F205VBT on some boards I developed.

Software development is done under Win7/x64 using Eclipse (4.4.1) with CDT (8.5.0),
Toolchain is gcc 4.8.4. (arm-none-eabi).

My Software Project is created with STM32CubeMX 4.6.0. and utilizes the HAL.
Works fine so far, but the CRC peripheral is missing from the configuration tree in CubeMX, when building a configuration for the STM32F2xx family.

CRC peripheral is supported for every other MCU family I tested, but is just missing for the one I'm using in this project.

Is there anything I could do to include the HAL driver for the CRC peripheral into my STM32F205 project?

Best regards,
Thorsten

Outcomes