AnsweredAssumed Answered

IAR Kickstart STM8L05 EEPROM

Question asked by schoeman.andre on Feb 4, 2014
Latest reply on Feb 5, 2014 by schoeman.andre
Hi

I'm using the 8K limited IAR Kickstart compiler on the STM8L051F3 (8K)

I'm using EEPROM and get the following 3 Linker errors

Error[Li005]: no definition for "__eeprom_program_byte" [referenced from eeprom_util.o(dlstm8smn.a)]
Error[Li005]: no definition for "__eeprom_wait_for_last_operation" [referenced from eeprom_util.o(dlstm8smn.a)]
Error[Li005]: no definition for "__eeprom_program_long" [referenced from eeprom_util.o(dlstm8smn.a)]

The functions are not mine. They are IAR library functions.

Does the Kickstart compiler support EEPROM?

Is there a special include file needed for EEPROM?

I've scanned through the General and Linker options and changed a few settings but to no avail.

Any suggestions?

Thanks
Andre




Outcomes