AnsweredAssumed Answered

Generate .hex for FlashLoaderDemonstrator with EWARM 6.70.1.5794

Question asked by RAPHAEL.PAESA on Feb 8, 2015
Latest reply on Feb 9, 2015 by RAPHAEL.PAESA
Hello,

I'm using IAR EWARM 6.70.1.5794 for developping a firmware on a STM32F107VCT6. I use a ST LINK V2 for debug. Now i would like generate an hex or bin file for downloading the file without ST-LIN V2 but with Flash Loader Demonstrator in bootloader mode. I have tried Project -> Options -> Output Converter -> Generate additional output file / Intel extended but when i try to load the file with Flash Loader demonstrator, i have an error : "unable to load this file..."
I have although tried to unselect "include debug information in output" but that's the same problem =(

Anyone have an idea to solve this?

Thanks

Outcomes