AnsweredAssumed Answered

STEVAL-IHM029V1 firmware built problem.

Question asked by bluecat on Oct 7, 2013
Hi.

I recently receive the STEVAL-IHM029V1 demo board, with the firmware code on a CD, I installed the STVD software and the COSMIC compiler I setup everything, but I can not get the firmware compiled, If there is somebody that could help me please.

the error I get on the STVD is:

Running Linker
clnk -m Debug\ihm029_v1.map -l"C:\Program Files\COSMIC\CXSTM8_32K\Lib"  -o Debug\ihm029_v1.sm8 Debug\ihm029_v1.lkf
#error clnk Debug\ihm029_v1.lkf:1 no default placement for segment .Signature
 The command: "clnk -m Debug\ihm029_v1.map -l"C:\Program Files\COSMIC\CXSTM8_32K\Lib"  -o Debug\ihm029_v1.sm8 Debug\ihm029_v1.lkf " has failed, the returned value is: 1
exit code=1.

ihm029_v1.elf - 3 error(s), 0 warning(s)

I would appreciate any help.

Thanks in advance.

Outcomes