AnsweredAssumed Answered

Looking for an STM8 evaluation board with 6K of RAM

Question asked by Philipp Krause on Sep 2, 2013
Latest reply on Sep 4, 2013 by Philipp Krause
So far I have used an STM8L-discovery, but the 1K of RAM is not enough any more. I need 6K. Otherwise I just want an LED or two, some GPIO and a serial port.

Any recommendation?

Philipp

P.S.: There is this STM8/128_EVAL bord. However the descriptions don't mention with which microcontroller it comes. The photo in the manual looks as if there was a ZIF socket for the microcontroller, so I would have to buy one separately, but the boards on ebay seem to have a microcontroller soldered.

Outcomes