AnsweredAssumed Answered

STM8 USING STVD & COSMIC COMPILER #error clnk Debug...

Question asked by nelson.greg.002 on Aug 10, 2013

Can anyone help me with the problem below dotted line?  It seems like I need to set up memory spaces for the Micro Controller.  Is that ? the problem.  If so how do I fix? Thanks! GDN

-------------------------------------------------------------

Running Linker

clnk -l"C:\Program Files\COSMIC\Lib" -o Debug\i2c_iap.sm8 -mDebug\i2c_iap.map Debug\i2c_iap.lkf

#error clnk Debug\i2c_iap.lkf:1 no default placement for segment .MAIN_CODE

#error clnk Debug\i2c_iap.lkf:1 no default placement for segment .SPI_CODE

#error clnk Debug\i2c_iap.lkf:1 no default placement for segment .CLK_CONST

#error clnk Debug\i2c_iap.lkf:1 no default placement for segment .CLK_CODE

#error clnk Debug\i2c_iap.lkf:1 no default placement for segment .I2C_CODE

#error clnk Debug\i2c_iap.lkf:1 no default placement for segment .I2C_CONST

#error clnk Debug\i2c_iap.lkf:1 no default placement for segment .GPIO_CODE

#error clnk Debug\i2c_iap.lkf:1 no default placement for segment .FLASH_CODE

The command: "clnk -l"C:\Program Files\COSMIC\Lib" -o Debug\i2c_iap.sm8 -mDebug\i2c_iap.map Debug\i2c_iap.lkf " has failed, the returned value is: 1

exit code=1.

Outcomes