AnsweredAssumed Answered

Deviation in AWU clock frequency

Question asked by WoRo on Aug 7, 2013

I'm using the BEEP function of my STM8S105, but it doesn't work as expectet.  It's not that I need the exact frequency, but I want to know, why it differs from the correct vallue, when chosing HSE as timebase.

Basic settings:
- external quartz crystal 16MHz
- MCU options:
   EXTCLK: External Oscillator (OPT4 EXTCLK = 0)
   PRSC: 16MHz to 128kHz (OPT4 PRSC[1:0] = 00)
- BEEP_CSR = 0xCE

1st test:
 option CKAWUSEL: High Speed External (OPT4 CKAWUSEL = 0)
-> expected fBEEP: 4kHz; real result: 2.69kHz :o(    ????

2nd test:
- option  CKAWUSEL: Low Speed Internal (OPT4 CKAWUSEL = 1)
-> expected fBEEP: 4kHz; real result: 4.09kHz :o)

Any clue???

TIA,
WoRo

Outcomes