AnsweredAssumed Answered

Does ST-LINK Utility support multiple devices on JTAG chain?

Question asked by kutscha.tim on Jan 7, 2015
Latest reply on Jan 12, 2015 by S C
I have a system with multiple STM32F407 MCUs.  The JTAG signals are daisy-chained together into one long chain.

Can I use the ST-LINK Utility to flash firmware into a specific device on the JTAG chain?  I looked through the user manual but did not find any settings to select which device on the JTAG chain to program.

I'm able to do this with a different hardware pod (J-Link from Segger), but I was hoping to use the ST-LINK/V2 pod since it costs 90% less.

Thanks for your time!
Tim

Outcomes