AnsweredAssumed Answered

Define segment option -ck for interrupt vector using STVD (COSMIC)

Question asked by tien.michael on Dec 21, 2012
Latest reply on Jun 3, 2013 by tien.michael
I am using COSMIC compiler in STVD.  I try to define segment option -ck for all program and constant.  I can use Project Settings->Linker->Input->Segment/Section to add option for all .const and .text.  But the interrupt vector is not included for this option -ck.  
I check the .lkf file generated by STVD, interrupt vector is generated like

# Interrupt vectors file - section reserved for STVD
#<BEGIN VECTOR_FILE>
+seg .const -b 0x8000 -k
Release\stm8_interrupt_vector.o
#<END VECTOR_FILE>


Is there a way to add more option to the generate script for interrupt vector?  I don't see anywhere to add options.

Thanks
Michael Tien

Outcomes