AnsweredAssumed Answered

TNeo: stable open source real-time kernel with well-formed code and detailed tests (for Cortex-M0/M0+/M3/M4/M4F)

Question asked by frank.dmitry on Jan 2, 2015
Latest reply on Mar 17, 2015 by frank.dmitry
I'd like to present real-time kernel: TNeo.

TNeo was born as a thorough review and re-implementation of TNKernel. The new kernel has well-formed code, inherited bugs are fixed as well as new features being added, it is well documented and tested carefully with unit-tests.

Currently it is available for the following architectures:
       
  • ARM Cortex-M cores: Cortex-M0/M0+/M1/M3/M4/M4F (supported toolchains: GCC, Keil RealView, clang, IAR)
  •    
  • Microchip: PIC32/PIC24/dsPIC

Comprehensive documentation is available in two forms:

Short list of features can be found here.

Outcomes