AnsweredAssumed Answered

stm32f429 discovery - usb mini-type B - Need functionality similar to nucleo boards

Question asked by Jimmy on Dec 30, 2014
Latest reply on Jan 8, 2015 by Jimmy
Hello,

The Nucleo usb mini-type B(CN1) has the following functionality:

1. st/link
2. serial port
3. mass storage device to allow application flash upload to the board.

I would like to have this same functionality on the mini usb type-B(CN1) stm32f429 discovery board. Is there a bootloader for the stm32f429 discovery that could provide this same functionality? The setup of both boards seems fairly similar with regards to the stm32F10 chip attached to the mini usb.  Is there anything preventing this on the stm32f429 from a hardware perspective? If anybody could give me some pointers it would be helpful.

Thanks,

-jimmy

Outcomes