AnsweredAssumed Answered

Problem to build example with iar 7.4

Question asked by modjo on Mar 24, 2016
Latest reply on Apr 1, 2016 by Gigi
Hi, i have some problems to build a project for P-Nucleo IHM001_singledrive kit !

When i open the project it said me that some options are broken and when i build the project (after use workbench tool to configure the motor) i have this error :

startup_stm32f302.s 
Error[438]: This instruction is not available in the selected cpu/core C:\Program Files (x86)\STMicroelectronics\FOC SDK\STM32 PMSM FOC LIBv4.2\Common\Libraries\CMSIS\CMSIS_2_x\Device\ST\STM32F30x\Source\Templates\iar\startup_stm32f302.s 173 
Error while running Assembler 
arm_biquad_cascade_df2T_f32.c  
Fatal Error[Pe1696]: cannot open source file "arm_math.h" C:\Program Files (x86)\STMicroelectronics\FOC SDK\STM32 PMSM FOC LIBv4.2\Common\Libraries\CMSIS\CMSIS_2_x\DSP_Lib\Source\FilteringFunctions\arm_biquad_cascade_df2T_f32.c 41 


Can you help please ?






Outcomes