AnsweredAssumed Answered

Can't get ST-Link driver to work on Windows XP, help??

Question asked by clfit.michael on May 29, 2012
Latest reply on May 31, 2012 by clfit.michael
Hi,
I have a couple of these:
http://www.st.com/internet/evalboard/product/250863.jsp

I am trying to get the on board ST-Link programmer to work with windows XP.
I have installed the WinXP SW driver from here:
http://www.st.com/internet/evalboard/product/219866.jsp

And I'm having no luck, my board works fine on a Windows 7 machine, and the ST-Link utilty reports my device firmware as "V1.J12.S0 JTAG Debugger"

When I connect the device for the first time (or after deleting it's registry enum), Device Manager shows ST-LINK momentarily as an unknown device, then it vanishes, and only the USB Disk Drive "STM32" remains. The USB drive with the 3 web links on it works fine.

I have tried the ST Visual programmer, the ST-Link utility, and CoFlash (Cocox), all say they cannot connect to the programmer.

Any help would be greatly appreciated.

Regards, Mick.

Outcomes