AnsweredAssumed Answered

Problem with CubeMX 4.5.0

Question asked by Dimitris Paraskevopoulos on Dec 11, 2014
Latest reply on Jan 9, 2015 by STM32Cube-T
I would like to point out the problems that I have encountered with CubeMX thus far.

I am trying to set up an SPI communication between an STM32F401RE Nucleo board (Master) and an mbed LPC1768. I tried using the CubeMX code generator and export it into Keil 5 but I couldn't load the program.

Even though I chose the correct board when trying to setup the code when the code was generated and loaded into Keil it reported a different Target name.

I tried to change the target options to the STM but it didn't work.

Has anyone else had the same problem?

Outcomes