AnsweredAssumed Answered

How to compile examples from the FOC library using KEIL.

Question asked by wolff.roger on Dec 26, 2015
Latest reply on Jan 10, 2016 by wolff.roger
Hi, 
Not getting anywhere with GCC I've gone ahead and installed windows, keil, cube and the FOC development kit. 

When I follow STM's howto for compiling the example, keil reports: "undefined symbol: R3_1_F3xx_NewObject"

This symbol is defined in the Web/Project/MDK-ARM/MC_Library_Compiled/Exe/MC_Library_STM32F302x8_single_drive.lib library. 
And... under project->manage->project items I see   MC_Library_STM32F302x8_single_dri listed in the third column. Apparently the windows8 window-manager does not allow me to increase the size of that window, so I must assume that the last two letters are there. 

So: How do I check that this library is actually used, and/or how do I find out why it isn't finding this symbol?

Outcomes