AnsweredAssumed Answered

Defining table in Flash instead of RAM, IAR

Question asked by healy.cyrus on Jun 11, 2012
Latest reply on Jun 13, 2012 by healy.cyrus
Hello,
Wondering if anyone has been able to use IAR to put a table in ROM memory instead of the default RAM with init table.  I would like something like: code int a[] = {1,2,3,4,5,6} or int a[] @ "abc" = {1,2,3,4,5}, where abc could be defined in the linker.
Thanks,
AlphaWolfXV

Outcomes