AnsweredAssumed Answered

STM8S UART Speed

Question asked by stevens.mark on Jun 4, 2012
Latest reply on Jun 5, 2012 by stevens.mark
I am using the UART1_Printf example from the STM8S Standard Peripheral Library version 2.1 and I am having problems with the speed of the UART.  I am expecting to see 115200 baud but according to my logica analyser I am in fact seeing  53 baud (approx).

To double check the LA value I have fed the output from an independent system running .NETMF and asked it to produce a similar signal.  The LA reports the right baud rate give or take a small deviation (i.e. 9615 baud).

Is anyone else seeing similar problems or have a solution?

Regards,
Mark

Outcomes