AnsweredAssumed Answered

Problem with clock configuration of NUCLEO-L152RE using STM32Cube

Question asked by amadei.angelo on Nov 21, 2014
Latest reply on Nov 25, 2014 by wahl.juergen
Hello, I'll be glad to recibe any help.


I've created a project for the NUCLEO-L152RE using STM32Cube (selecting the correct board) and then I've exported it to IAR-EWARM. When I run the project into the board, the MCU don't continue after the clock configuration. If I go step by step over the code, when the HSI clock is set, all stops.


The configuration clock option was: HSI RC (16MHz) --> PLLCLK (x4 /2) --> SYSCLK (32MHz). All the other configurations by default.


I'll appreciate any help! Thanks! 

Outcomes