AnsweredAssumed Answered

Motor in did not stop timing, immediately start processing

Question asked by cheung.jacky.001 on Jan 24, 2015
Latest reply on Mar 20, 2015 by Gigi

Gigi:
     
       I have to ask a question, I driver the motor for FOC sensorless, speed of 30 - 162 RPM, the motor can start colse_loop now, but because of the shutdown, and sometimes motor inertia, not stopped down, then if immediately start, will start failure, is excuse me this kind of, also has in the motor inertia, no stop timing, and then start. In this situation, how to deal with?

       Best Regards
          Jacky

Outcomes