AnsweredAssumed Answered

openocd

Question asked by kantardzioski.filip on May 3, 2012
Latest reply on Jul 31, 2012 by sjo
Hi all,

i want to configure OpenOCD for Stlink(embedded on stm32vld board)...

but after building and starting openocd i've got this output:

01.openocd -f /usr/local/share/openocd/scripts/interface/stlink-v2.cfg - f /usr/local/share/openocd/scripts/target/stm32f1x_stlink.cfg help
02.Open On-Chip Debugger 0.6.0-dev-00477-gf1c0133 (2012-05-03-11:07)
03.Licensed under GNU GPL v2
04.For bug reports, read
06.Warn : must select a transport.
07.1 kHz
08.trst_and_srst separate srst_gates_jtag trst_push_pull srst_open_drain
09.Info : clock speed 1 kHz
10.Error: session's transport is not selected.
11.in procedure 'transport'
12.in procedure 'init'

openocd version is 0.6.0....jumpers on the board are OK....i am using Ubuntu 11.04....

should i add some extra commands in command line to select transport or should i edit .cfg files??

Thanks,

Filip.

Outcomes