AnsweredAssumed Answered

Best bluetooth module to use

Question asked by corregedor.antonio on Apr 29, 2012
Latest reply on May 9, 2012 by corregedor.antonio
Hi all,

I am currently using the STM3210C evaluation board to implement a prototype for a project I am currently busy with, and I am at the point where I need to add Bluetooth capability to my board.  In essence what I am trying to achieve is to stream the data from the STM3210C to another computer which is situated away from the STM3210C.

I was thinking of using a Bluetooth module as from what I can see on the net, there are Bluetooth modules which can be used to make "wireless serial cables".  So the idea is to use my eval board to interface to a Bluetooth module using the USART (RS232); and then pair the Bluetooth module to my laptop to get the information off the eval board.

I was hoping that this forum could point me towards an appropriate module which someone has possibly used in a project before, and that is easy to interface with the STM32 range.  Thanks in advance for any help which you guys can offer.   

Regards,
  Tony

Outcomes