AnsweredAssumed Answered

Bluenrg-1 DTM failing

Question asked by jamp on Jul 9, 2018

Hello all,

I am using the DTM for bluenrg-1 I can program the unit and it will work fine but for some reason when the unit is left powered down for a couple of hours and then powered up again some times stops working.
Doing a flash reading starting in address 0x10040000 I can see the next difference:

On the unit that is working:

00 60 00 20 61 16 04 10 29 18 04 10 39 18 04 10

 

On the unit that stops working:

00 00 00 20 61 16 04 10 29 18 04 10 39 18 04 10

 

For some reason that byte changes value.

Any idea why that problem could happen.

 

Thank you

Outcomes