AnsweredAssumed Answered

F091_Cube_FW: Connect a wire between PA4 and PA4...

Question asked by Juergen Marquardt on Jul 5, 2018
Latest reply on Jul 6, 2018 by waclawek.jan

Diving into STM32F091 Nucleo  Examples (STM32Cube_FW_F0_V1.9.0).

Trying ADC Sequencer and find this comment in main.c:

 

#if defined(WAVEFORM_VOLTAGE_GENERATION_FOR_TEST)
/**
  * @brief  For this example, generate a waveform voltage on a spare DAC
  *         channel, so user has just to connect a wire between DAC channel
  *         (pin PA.04) and ADC channel (pin PA.04) to run this example.
  *         (this prevents the user from resorting to an external signal generator)
  *         This function configures the DAC and generates a constant voltage of Vdda/2.
  *         To modify the voltage level, use function "WaveformVoltageGenerationForTest_Update"
  * @param  None
  * @retval None
  */
static void WaveformVoltageGenerationForTest_Config(void)

 

Besides being unable to connect PA4 with PA4 (DACOUT1 and ANIN4 are both at PA4), two questions:
   - Is there any detailed structure doc of e.g. STM32F091 pin PA4 (AIN4 and DACOUT1) regarding ADC and DAC ?

   - Is it possible to read a DAC back via AIN if they share the same pin (PA4 in my case)?

Juergen

Outcomes