AnsweredAssumed Answered

Linker problem "symbol d_imul not defined"

Question asked by Eric Stark on Nov 4, 2011
Latest reply on Dec 1, 2011 by inler
I'm building a project for an STM8S208 using the Cosmic compiler (CXSTM8_32K) within ST Visual Develop.  When I link, I receive the error "symbol d_imul not defined".  The project was working well previously using only 8-bit operations, but I recently added some 16-bit multiplication operations.  Do I need to link in an additional math lib to support 16-bit (or 32-bit, for future reference) operations?

Outcomes