AnsweredAssumed Answered

BlueNRG-2 | Unable to debug over STLINK/V2 | Multiple Issue

Question asked by ANSHUMAN TRIPATHI on Jun 28, 2018

Hi All,

Please help I'm stuck with this, I am currently having some difficulties while programming and debugging the BlueNRG-2 "STEVAL-IDB008V2" over STLink/v2.

 

PROBLEM FACED : When trying to debug and flash the code using TrueStudio getting following error message
Failure at line:13 in 'Target Software Startup Scripts'. Please edit the debug configuration settings. Error writing data to flash

 

 

Details:

Board : STEVAL-IDB008V2
BlueNRG2 Part Number :[/b] BLE232ES
IDE Version : Version: 9.0.1, Build id: 20180420-1214
Project : Imported from BlueNRG-2 Navigator Examples
Example : BLE_SensorDemo_BlueMSapp
Build Status : Success
Hardware Test : OK - Tested by flashing code using :
1. BlueNRG-2 Navigator over USB-Serial, and
2. BlueNRG-1 ST-Link Utility over STLINK/V2.

 

Additional Information:

Console Message while debugging

Atollic TrueSTUDIO gdbserver for ST-Link. Version 4.2.2 (WIN32 2018-02-26 16:20:21 15675)
Copyright (c) 2018, STMicroelectronics. All rights reserved.


Starting server with the following options:
Persistant Mode : Disabled
LogFile Name : debug_log.txt
Logging Level : 31
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Enabled
SWD Debug : Enabled

Atollic TrueSTUDIO gdbserver for ST-Link. Version 4.2.2 (WIN32 2018-02-26 16:20:21 15675)
Hardware watchpoint supported by the target
STM32 device: Flash size =256
Enter STM32_AppReset() function
NVIC_DFSR_REG = 0x00000009
XPSR = 0xC1000000
ST_LINK Major version =2 Jtag version =31
ST_LINK VID=1155 PID=14152
ST_LINK device status: HALT_MODE
ST_LINK detects target voltage =3.24 Volt
ST-Link device initialization OK
Waiting for debugger connection...
Waiting for connection on port 61234...
Accepted connection on port 61234...
Debugger connected
ST_LINK device status: HALT_MODE
Reading 0x4 bytes of memory from addr 0x100006fa
Reading 0x2 bytes of memory from addr 0x100006fa
Enter STM32_AppReset() function
NVIC_DFSR_REG = 0x00000009
XPSR = 0xC1000000
Flash erase: Address= 0x10040000, Length=92160
Flash write: Address= 0x10040000, Length=192
Programming flash..
STM32 device: flash programming successful 0x10040000
Flash write completed in 0.198000 seconds, 0.946970kB/s
Flash write: Address= 0x100400c0, Length=2944
Programming flash..
STM32 device: flash programming successful 0x100400c0
Flash write completed in 0.301000 seconds, 9.551495kB/s
Flash write: Address= 0x10040c40, Length=2960
Programming flash..
STM32 device: flash programming successful 0x10040c40
Flash write completed in 0.305000 seconds, 9.477459kB/s
Flash write: Address= 0x100417d0, Length=2944
Programming flash..
STM32 device: flash programming successful 0x100417d0
Flash write completed in 0.304000 seconds, 9.457237kB/s
Flash write: Address= 0x10042350, Length=2944
Programming flash..
STM32 device: flash programming successful 0x10042350
Flash write completed in 0.307000 seconds, 9.364821kB/s
Flash write: Address= 0x10042ed0, Length=2944
Programming flash..
STM32 device: flash programming successful 0x10042ed0
Flash write completed in 0.311000 seconds, 9.244373kB/s
Flash write: Address= 0x10043a50, Length=1896
Programming flash..
STM32 device: flash programming successful 0x10043a50
Flash write completed in 0.275000 seconds, 6.732954kB/s
Flash write: Address= 0x100441b8, Length=108
Programming flash..
STM32 device: flash programming successful 0x100441b8
Flash write completed in 0.202000 seconds, 0.522123kB/s
Flash write: Address= 0x10044224, Length=48
Programming flash..
STM32 device: flash programming successful 0x10044224
Flash write completed in 0.264000 seconds, 0.177557kB/s
Flash write: Address= 0x10044254, Length=124
Programming flash..
STM32 device: flash programming successful 0x10044254
Flash write completed in 0.204000 seconds, 0.593597kB/s
Flash write: Address= 0x100442d0, Length=66
Programming flash..
STM32 device: flash programming successful 0x100442d0
Flash write completed in 0.214000 seconds, 0.301183kB/s
Flash write: Address= 0x10044312, Length=16
Flash write completed in 0.057000 seconds, 0.274123kB/s
Reading 0x20 bytes of memory from addr 0xf0000fd0
Reading 0x4 bytes of memory from addr 0xffffffff
Reading 0x4 bytes of memory from addr 0xffffffff
Enter STM32_AppReset() function
NVIC_DFSR_REG = 0x0000000B
XPSR = 0xC1000000

 

Startup Scripts -> Target Software Startup Scripts

# Set flash parallelism mode to 32, 16, or 8 bit when using STM32 F2/F4 microcontrollers
# Uncomment next line, 2=32 bit, 1=16 bit and 0=8 bit parallelism mode
#monitor flash set_parallelism_mode 2

# Set character encoding
set host-charset CP1252
set target-charset CP1252

# Reset to known state
monitor reset

# Load the program executable
load

# Reset the chip to get to a known state. Remove "monitor reset" command
# if the code is not located at default address and does not run by reset.
monitor reset

# Enable Debug connection in low power modes (DBGMCU->CR)
set *0xE0042004 = (*0xE0042004) | 0x7
# Set a breakpoint at main().
tbreak main

# Run to the breakpoint.
continue

Outcomes