AnsweredAssumed Answered

Can create the 1 us period with the timer 2 of  STM8L051F3 ?

Question asked by edmond yun on Jun 28, 2018
Latest reply on Jun 29, 2018 by Clive Two.Zero

Hello, 

 

I would like to make 1 us period with timer 2 of STM8L051F3.

currently I checked that 1 ms is correct, if trying to use under 1 ms (like 100 us or 10 us), the period is not correct....

I measured the period with GPIO(LED).....

 

please help to let me know whether can make 1 us period with timer 2 or not..

and if has another solution, please help to provide the example with detailed information...

 

thankful for your support in advance,

 

thanks.

Outcomes