AnsweredAssumed Answered

Motor electrical parameters

Question asked by boeh.frank on Oct 24, 2014
Latest reply on Oct 27, 2014 by boeh.frank
Hi,

I am not entierly sure how to correctly enter my motor parameters, and which effect they have, can anyone check if I am doing this correctly (sensorless operation with cordic startup, no extra features like flux weakening, bus voltage sensing):

- max rated speed: used for fault detection only, correct?
- nominal current: used for torque limitation, correct?
- nominal dc voltage: what is this value used for?
- Rs: this is meant per leg, so I measure the DC resistance between two phases and divide this by two
- Ls: same as Rs, measured at 100Hz
- demagnetizing current: what is this value used for?
- B-EmfConstant: I drive the motor externally, measure the AC voltage between two legs, calculate the RMS from that, divide this by used RPM, multiply with 1000

Any help is appreciated.

Regards
Frank

Outcomes