AnsweredAssumed Answered

SPSGRF-868 module

Question asked by GUNA SEKARAN on Jun 21, 2018
Latest reply on Jun 24, 2018 by GUNA SEKARAN

I am using SPSGRF-868 module on a medical device. I am trying to get the connection established between acquisition board(transmitter) with the Main display board (receiver). Both have this module configured in P2P mode.

 

I used a code base from STM32CubeExpansion_SUBG1_V2.0.0 - I am using F4 controller @ both sides.

Essentially same code base.

 

HAL_Spirit1_Init();

P2P_Init();

Seems to do its job. Confirmed SPIs CLK and other things.

P2P_Process @ receiver side does not receive anything. Perhaps, sending is not proper. Not sure.

 

I am setting state machine to SM_STATE_START_RX for receiving and SM_STATE_SEND_DATA for transmitting before P2P_Process call.

 

Only change in my implementation is GPIO IRQs (Tx/Rx) are not configured. In my board the module GPIOs(all 4)are grounded and NOT connected to processor. Is it necessary to connect and configure for this code base to work?

 

Looking forward..

Thank you

Guna

Outcomes