AnsweredAssumed Answered

Motor Electrical parameters Rs and Ls

Question asked by cheung.jacky.001 on Oct 21, 2014
Latest reply on Oct 23, 2014 by cheung.jacky.001
Gigi:
       I have a question, measured in workbench Motor Electrical parameters Rs and Ls. I see ST data is used RLC meter measurement frequency at 100 Hz, but the motor is running in the PWM 16K frequency, whether I used RLC meter frequency measurement of 10K or 100Hz? Because both the difference between the value of high. And RS is using a multimeter to measure, or with the corresponding RLC frequency? 
       Best Regards
          Jacky

Outcomes