AnsweredAssumed Answered

LIS2DW12 INT1?

Question asked by vitthal muddapur on Jun 15, 2018
Latest reply on Jun 19, 2018 by Miroslav B

Hi,

1. Write 64h in CTRL1 // Turn on the accelerometer // ODR = 200 Hz, High-Performance

2. Write 04h in CTRL6 // FS 2 g LOW_NOISE enabled

3. Write 20h in CTRL7 // Do not use low-pass filter for 6D, enable interrupts

4. Write 40h in TAP_THS_X // Set 6D threshold (6D_THS[1:0] = 10b = 60 degrees)

5. Write 80h in CTRL4_INT1_PAD_CTRL // 6D interrupt driven to INT1 pin

 interrupt set in SIXD_SRC register but didn't get any interrupt from INT1 

Outcomes